I have attached a picture of what I am needing. I believe it is closest to 0022013047. I only need two of these and any other items that would help me get the wires connected. Unless they come with a set of pigtails attached. I need at least 5” of wiring any color. Any help would be appreciated.
Hello JimS, welcome to the TechForum.
We would not have pigtails for this one. Just the contacts for it. See link below for contacts.
Hi JimS,
Assuming that the 0022013047 is indeed the right part (the pitch on that connector is 0.1", or 2.54mm), then this link will provide you various options for jumper wires of at least 5" with the appropriate contact crimped onto one or both ends and offered in various wire gauge and color options.
David,
Thank you for the information.