10k MF filter capacitor

------Question for LLS1K103MELC Please Put your question below------

I need 10 capacitors for my audio amplifier. The current ones are 10000mF/80V in a can size of 35/50mm. The current capacitor I have has 2 leads for a snap-in soldering.

Is this the correct part number ? I had ordered a similar going my diagram and the datasheet but on receipt I found that it has 5 leads and won’t fit in my case. So can anyone give me the correct part number ? The min rated V should be 80V or above and the dimensions 35/50mm as there is not much space for taller caps

Hello, welcome to the TechForum!

It looks like this one will have 2 prongs like you need, but a slightly higher max height of 52mm if that can still work for you. Everything else looks like it matches.

1 Like