30P06k mosfet

looking for a similar version that will work

AM30P06-40D found this.

Hello itronic, this item: 3141-G230P06KCT-ND comes up when searching for the original number. Without details on specifications, this is the closest option that is in stock. If your application uses less than 29A, then AM30P06-40D is pretty comparable to G230P06K. However, the original can handle up to 60A maximum under the right conditions.

The 30 would be for 30A, the P for a P-Channel Mosfet, and the 06 for 60V.
I found a part number 353-MCU30P06Y-TPCT-ND, which may work for you.
There is also a part number 3141-G230P06KCT-ND, which can handle 60A of power.
Please check the datasheets to verify compatibility to your application.

Thank you very much. These will work.