Question: Is the calibration for 5880-FMA1804A-ND ISO 17025 compliant?
Answer: No, this has an NIST traceable certificate of calibration, which is not considered the same standard. It is also worth noting that “Factory Calibration” is not going to be the same as either of these standards, ISO and NIST standards must be certified, and the certificate must be confirmed before the product is shipped.