------Question for 7927A 0102000 Please Put your question below------
The stock you have (1664) is meters or spools?
Thank you
------Question for 7927A 0102000 Please Put your question below------
The stock you have (1664) is meters or spools?
Thank you
Hello ricardo.cunha,
The stock of 7927A 0102000 is neither in meters nor spools but in feet.
It is ordered per foot. 1 = 1 foot. It is supplied on a Digi-Spool with the maximum continuous spool size of 2000ft which would then be supplied in the manufacturer’s original spool if you wanted 2000ft. We currently only have 1,664ft in stock at this time so not a full manufacturer spool.
Regards.
The difference between those two part numbers is the length of the spool and the fact that 7927A 0101000 has to be ordered in quantities of 1000, which is 1000ft not meters, while 7927A 0102000 can be ordered less than 1000ft and up to 2000ft continuous. They are the same cable they just come on different size spools. Manufacturers often make more than one size of a spool of same cable, and we modify the length of 7927A 0102000 so that customers can order less than the full spool if they don’t need that much. The 7927A 0101000 is not modified and has to be ordered in multiples of 1000 quantity which stands for 1000ft.
I hope that explains it.