We got below questions from CSA about above Littlefuse switch#59070-4-S-02-F , would you please help contact manufacture to obtain the answer?
if the switch is:
potted inside the enclosure,
consists of a pair of ferromagnetic flexible metal contacts in a hermetically sealed glass envelope
with a glass to metal pins sealing
If they can’t answer above questions, they could send a picture of the sealing between the glass envelope and the pins, this should be sufficient for CSA to accept it.
Thanks
Hello @valerie.yang,
I’ve have sent your questions to Littelfuse and will update this thread when I receive their answer.
Hello @valerie.yang, Littelfuse confirmed the following for the 59070-4-S-02-F:
- It is potted with 2-part epoxy.
- It uses a pair of ferromagnetic flexible metal contacts in a hermetically sealed glass envelope.
- The glass is fully sealed to the metal reed contacts.
Littelfuse also provided the datasheet for the reed switch inside it, the MDRR-DT.
Littelfuse-Reed-Switches-MDRR-DT-Datasheet.pdf (301.2 KB)
Best regards!