It is important to review the datasheet of an AC fan upon ordering to see if there is an external capacitor requirement for the fan in order to operate.
These are typically not needed for the tubeaxial fans, but become more of concern when looking at other styles such as a motorized impeller type like below:
As examples, below are a couple of fans that do not come with a capacitor. I’ve listed a wet metal case option for each but generally speaking a different capacitor can also be used as long as it is rated for equal or higher voltage (220V for these fans) and the appropriate uF rating.
Note: Fully discharge the capacitors before working on a device, they store power during and after unit is off and supply is disconnected.
R4E400-AP15-10-ND
Click here for capacitor 381-2606-ND
381-3555-ND
Click here for capacitor 381-2605-ND
Boot is below if needed for either capacitor (450 series):
381-2591-ND
See Also:
Capacitor for EBM-Papst Fan D2E097-CB11-32
Summary
R4E400-AP15-10
2266-R4E400-AP15-10
450-20-0034
381-2606
450200034
2266-450-20-0034
450-20-0034-ND
450-20-0034-NDR
R4E355-AN09-10
R4E355
381-3555
R4E355-AN09-10-ND
450-20-0033
450200033
381-2605
2266-450-20-0033
450-20-0033-ND
450-20-0033-NDR
710-00-0042
381-2591
710-00-0042-NDR
710000042
710-00-0042-ND
ebm-papst
ebm papst