AHR40316FMW

------Question for AHR40316FMW Please Put your question below------

What is the designation for the leads on this one?

The data sheet reads:
Black: Input COM
White: Input Voltage 1
Red: Input Voltage 2
Blue: Input Voltage 3
Yellow: 24VAC Output

But there is no breakdown on what lead is for what, or if there are center taps, multiple taps per winding or what.

Can anyone provide me some idea?

Hello,

Welcome to the TechForum.

I was able to locate a bit of information to try assist. I see the Black and White are the Primary with the red and blue being the secondary. This is pretty set at the outputs and voltages.

Voltage - Primary
575V
Voltage - Secondary (Full Load)
24V
Current - Output (Max)
1.67A
Primary Winding(s)
Single
Secondary Winding(s)
Single
Center Tap
No
Power - Max
40VA

Thank you
Ryan

Since the transformer you’re asking about has a single primary input it’s just going to have the Black Common and White Input Voltage 1 and then two Yellows for the 24VAC output.

There is not going to be a center tap on this secondary.

That explains what I needed to know. Thanks.

1 Like