# Alternative for LEG75W-142-C0530 LED Driver

**URL:** <https://forum.digikey.com/t/alternative-for-leg75w-142-c0530-led-driver/10264>\
**Category:** Power Supplies (off-board)\
**Tags:** power-supplies-external-internal-off-board, cross-reference, power, thomas-research-products\
**Created:** [November 19, 2020, 6:47pm UTC](https://forum.digikey.com/t/alternative-for-leg75w-142-c0530-led-driver/10264 "2020-11-19T18:47:05Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![jeremy\_wiskow](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/jeremy_wiskow/32/25641_2.png) [@jeremy\_wiskow](https://forum.digikey.com/u/jeremy_wiskow)\
**Post date:** [November 19, 2020, 6:47pm UTC](https://forum.digikey.com/t/alternative-for-leg75w-142-c0530-led-driver/10264/1 "2020-11-19T18:47:05Z")

</div>

This LED driver is listed obsolete in our system. Here are some of the key specifications of the part:

- Type: Constant Current

- Voltage - Input (Min): 120VAC

- Voltage - Input (Max): 277VAC

- Voltage - Output: 48 ~ 142V

- Current - Output (Max): 530mA

- Power (Watts): 75W

With these specifications, we can find a possible substitute that has an active status.

These options can be considered similar to the original product - [LED Drivers](https://www.digikey.com/short/z0f9t0). These will have a similar power rating of 75W. There are multiple different output voltage ranges for these drivers, but they fit within the original range of the obsolete driver. This will depend how much voltage you would be using on the original voltage range. The output current on the recommended drivers are larger in max current, but will only supply the current needed, such as the 530mA.

Please also review the datasheets to make sure these will work for the application.

> The TechForum Cross Reference category is for parts that Digi-Key does not sell or parts that have gone obsolete. Our Engineers and Techs have reviewed the specifications for these parts and made a recommendation for a replacement. Please review the suggested part to ensure it will work for your application.