American Bright LED Strips Suffix Explanation

We often get feedback regarding strips like AB-FZC02440-19712-XA2-12S (2007-AB-FZC02440-19712-XA2-12S-ND) indicating that the parts are not actually 5000mm long. I reached out to American Bright for clarification. The datasheet does not explicitly call out the suffix after the main part number.

Suffix Explanation

You may see a few different formats depending on the part structure. This particular part uses “12S” to call out a 12" (300mm) length. Other strips may have a different call out, but if there is a suffix with three or two characters, “-XX; -XXX” this usually indicates that this is a pre-cut length to the number of inches called out in the numeric value provided. We are working on correcting some of the details for these parts, we apologize for the miscommunication.

1 Like