Any foot option?

------Question for 5855 BK005 Please Put your question below------

Hello, Is there any option for foot(ft) length option??

Unfortunately, it looks like we don’t have any per-foot options for that wire. I did a quick search and it seems that anything you look for with UL Style 1213 is going to be on spools of 100’ or more.

I see, is there any personal order available with per foot, or any alternatives with similar 19strands AWG22 PTFE Hook up Wire ?

There may be options available in other standards that meet those specs, is the specific UL and MIL standard listed in the original not as important?

Hi. Chris.

I found some Belden’s 83006, and it is said that it is TFE, not PTFE

Is there any difference between TFE and PTFE? I saw that both are same teflon..

Thanks,

That’s correct. Strictly speaking, TFE is the chemical used to create PTFE, but if it’s being used to describe a cable jacket they mean the same thing. In case there’s any doubt, the datasheet from Belden clarifies that the jacket material is PTFE for this wire: 83006 Technical Data Sheet