Arduino A000053 ISCP Header Pins Included?

------Question for A000053 Please Put your question below------

To whom it may concern,

Hi! I’m Jack from Talegent, and we are currently looking for new suppliers of the Arduino Micro A000053.

With past suppliers, the boards we received were missing the 6-pin ISCP header, which is important for our uses. This has been an issue with more than one supplier. If you could confirm that the boards you sell do have this 6-pin header, that would be fantastic! Then we would go ahead and continue our purchase through the regular avenues.

Thanks in advance,

Jack Egerton

Talegent

Hi @jegerton ,

Welcome to DigiKey TechForum and thanks for your inquiry.

Yes, the Arduino Micro A000053 does include the 6‑pin ICSP header

According to the official Arduino datasheet and store listing, the Arduino Micro (MPN: A000053) is manufactured and shipped with a populated 6‑pin ICSP (In‑Circuit Serial Programming) header as part of the standard assembly. The board description explicitly lists:

  • Micro‑USB connector
  • Reset button
  • 6‑pin ICSP header (2 × 3, standard AVR layout)

image

Hey Angus,

Thanks for getting back to me.

Because of the issues we’ve had with past suppliers selling these Arduinos without the pins (even though they are stated to be there in the datasheets, product description, and images) it would give us a lot of peace of mind if you could physically or visually confirm they are there. If aren’t able to do this, no worries! I appreciate you getting back to me anyways.

Kind regards,
Jack Egerton
Talegent

Hi jegerton,

In our Product Detail page for the A000053 version of the Arduino Micro, we have a “360°” image that our internal people took of the actual part.

If you click on that, you’ll find a 3D rotatable image of the actual part that we took out of inventory to image.