AU Plug

------Question for B496201 Please Put your question below------

Does this Product ship with an AU Plug.

Hello purchasing132,
Welcome to the TechForum, the part ships with a standard US 5-15P cord.

Note that this part can not take 230Vac on the input supply, even with a plug suited for the local wall outlet.

The only way to use this with 230Vac would be with a voltage converter which could convert the 230Vac down to 120Vac.

The datasheet states that there is another part number, the B496201-E, which takes 220 - 230 Vac, but we do not carry this variant.