AWM style 2080

Do you offer this UL spec 2080. It’s appliance wire. Here is the print on the existing cable

18/2 (.832mmsqrd) AWG E56702 AWM style 2080
105C 300V vw-1 CSA LL67880 AWM IA 105C 600v FT1

Hello,

I do not see any of the the UL 2080 in our system. The only appliance wire I see is from Remington. Here is a link: Remington Industries Single Conductor Cables (Hook-Up Wire) | Electronic Components Distributor DigiKey. These are a marketplace item which means they would ship directly from Remington. They might have other appliance wire though that we do not list.