I am in the middle of building a mini network rack and currently planning my power supply routing etc. the PSU would be a Mean Well NDR-480-48 dialled upto 54V, then the wires would be split using a junction box for 3 different devices, then running through a din mounted circuit breaker 1 per device, from each circuit breaker I would like to run the wire to a passthrough connector then onto the individual device’s.
I was thinking of using the following part numbers but am concerned that they are only rated at 48V and not 60V, the barrel plugs need to be 2.1mm x 5.5mm in size, center positive.
10-03672
10-00113
10-01776
would these parts work/be safe to use? if not what would you recommend?