BLE Message Based Triggering

------Question for 113991194 Please Put your question below------

Hi,

On this device, is it possible to configure to receive a bluetooth message to trigger sending the location information. In general, is it possible to receive a message and then based on that send the location information.

Thanks

Gopi

I’m not sure if you can configure it so that you can send a bluetooth message from, for example, a phone or PC to do this, but the associated tracker for this series can be configured to do just this.

If you set up 1597-114993106-ND correctly, you should be able to use it to receive location data whenever you press the button on the case. It will send a signal to 1597-113991194-ND and receive location information from the transmitter.

Chris,

Thanks for the information. Appreciate it.

In my use case, it will be another BLE tag that would have send the message to the device 1597-113991194-ND then the device send its location. Would this work?

Thanks

Gopi

Yes, it should work with another BLE device as long as it matches the communication parameters laid out in the datasheet: E5 Beacon Specifications

I can’t vouch for ease of use, but it should work with a variety of trackers according to Seeed’s documents.