We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
Maybe JST?
03KR-6S-P?
X Y Z
8.20mm * 4.80mm * 7.80mm
Pitch: 2mm
I am currently looking for the JST connector or another brand that can fit into a random piece of electronics.
I measured the outer XYZ parameters and then the pitch also like described. I also listed the match that I found but the datasheet for this part seems a bit vague unless I know the part well…
I wanted either a loose end of three wires with a connector of this type…
A connector and heat dissipative wiring harnesses
or… A connector with heat dissipative wiring and the crimps (either pre or I have to do it)
I know this is asking a lot. If you or your company’s personnel know of a way to get these items, please let me know.
I guess what I am asking is does this connector come as a pre-crimped model with three wires that are extremely long (over three feet) or can I get the connector(s), crimps, and a specific type of wiring from you and your company’s personnel?
Seth
P.S. Any advice for protective coatings for heat would be nice and if your company has these types of wiring, please let me know.
It’s not uncommon for contacts to lack any official recommendation for hand-operated tooling, since it’s unsuitable for production use. In those cases folks typically use generic tooling such as the 1528-5682-ND or WM9999-ND and make do with the lesser quality/consistency that results.
Those are the connectors I needed: XH from JST were the exact match or extremely close to the exact match. They seem a bit different but fit nice and snug.
Seth
P.S. And right about the pitch… I was unable to check with my current caliper well enough. I will keep looking at the Pitch of a Connector link you have listed. Thank you.
@heke and @rick_1976 , looking into this a bit further and remembering how to measure hole to hole gave me some ideas on small connector assemblies.
Outside to outside of neighboring holes: 3.00mm
Diameter of the hole(s): 0.6mm
Outside to Outside of neighboring holes - Half the Diameter of the hole(s) = ?
The answer should be very close with a caliper of +/- 2.7mm!
I did not take into account the half value of the entire Diameter of the hole(s) at first and then I remembered this simple formula. @heke , I read over the post listed that you provided.
I understand the rationale for it and I think with pins that are available, it could work well or does work well (either/or). I just got too used to using the caliper for hole measurements with Diameter and spacing between the holes furthest, neighboring extent.
Anyway, the parts that I ordered with the header XH type from JST work as is now. Thank you both for the heads up and data (and link for future, available pins that are male).