We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
------Question for DLPC4420AEVM Please Put your question below------
Dear Team, I would like to connect my DLPC4420EVM to the front end board of to the DLPC4420EVM (i.e. Part DLP064). May I know the specification of the cable needed for connecting the front end board, please? Is there any extra precaution for the projection pattern images via the HDMI port of the front end board ?
DLPC4420AEVM is equipped with FI-RE51S-HF connector, and FI-RE51S-VF is mounted on the front-end board DLP064(from DLPC4420AEVM Board Design Files).
They both can be connected with 51 positions JF08 series harness.
Could you also explain what you mean by “extra precaution for the projection pattern images via the HDMI port?” I’m not sure I understand that question.
My question is whether I can directly project images from my computer to the DMD using the HDMI port or whether I would need to use the DLPC44xx GUI software for this.
the 51POS JF08 cable is WRONG for connect front-end board!! Because I just used it and it corrupted my DLPC board!!! The connector pins in DLPC are actually mirrored with the pins in HDMI board, you actually need a reverse 51POS cable, not this standard one!!! WHAT AN IDIOT BOARD DESIGN!