Can this PS be configured to:

------Question for 73-778-022 Please Put your question below------

Can the 73-778-022 be configured to:

  • Use standard 120VAC wall power
  • Convert to DC 100V-10A
  • That could supply this to 12each PCB’s in a card cage?

Hello john.huedepohl and welcome to the DigiKey TechForum.

Unfortunately, looking at the modules on the manufacturers page and their brochure, it does not appear that this would have those options. I do not see that it has a 100V output option for a module and it lists the input range as 180VAC to 528VAC.