Can’t find part number BM04B-PAMUK-A-TB JST Automotive Connector
I am not seeing that we currently list the BM04B-PAMUK-A-TB.
How many were you looking to get a quote for?
Hi,
I am looking for 65pcs.
I will have a request for a quote for that item number to be submitted.
Have you already ordered the contacts?
The manufacturer lists the below two options for that housing.
SPAMU-002T-M0.5 for 26AWG
SPAMU-01T-M0.5 for 22awg
Also, a note.
We do list some pre-crimped wire leads for that housing too.
These use the SPAMU-01T-M0.5 for 22awg at different lengths.
Jumper Wires, Pre-Crimped Leads | Cable Assemblies | DigiKey
With the information available I have submitted to the quotes team a request to quote the connector housing, both of the contacts(for the different wire sizes) and the tooling I was able to find for each. Listed below were the items I had sent in that request
– BM04B-PAMUK-A-TB for the housing
– SPAMU-002T-M0.5 contact for 26awg
– SPAMU-01T-M0.5 contact for 22awg
– Tool YRS-1890 for the SPAMU-002T-M0.5 contacts
– Tool YRS-1870 for the SPAMU-01T-M0.5 contacts
You should hear from the quotes team. It can take a few business days if they need to ping the manufacturer for anything. If you need to check on the status of the quote please call the 1-800-344-4539 and ask to for an update on the quote.
The contacts and housing item numbers were verified by the data in the first link below.
JST web-page for the connector.
The tooling was found using the tool finder JST has on their site in the second link.
You would copy either item number for the contact above and use it in the search box found on the page.
Application Tooling Guide | Crimp Style | JST Sales America