I am looking for an SMD Hybrid / Polymer Aluminum Electrolytic Capacitor with the following specs: 4.7µF, 20% tolerance, 35V. I haven’t been able to find an exact match from standard manufacturers. Does anyone have a part number suggestion or a recommended alternative?
Greetings,
4.7uF and 35V are ratings at the lower end of the range serviced by electrolytic capacitor types, and newer/more novel types such as hybrid polymer devices tend to build out more from the center of the distribution where usages are higher.
Selection of an alternative should be guided by the reasons that an aluminum hybrid type was requested; size, cost, lifetime, typical failure mode, ESR, temperature stability, and frequency response are all potential factors of interest, and the balance of interests for the application in question is not apparent. There are quite a few standard aluminum capacitors with these values available, as well as a variety of tantalum polymer devices, and even some film products. Quite a few standard tantalum products and ceramics are available also, though using them successfully depends on understanding and accounting for some rather unpleasant behaviors that often come as a surprise to the uninitiated.