CM-7153 SPEC

-—WHAT IS THE STATIC OFF RESISTANCE–Question for 7153 Please Put your question below------

AND DATA SHEET ON THIS PART

Hello,

I was able to locate the datasheet and have it on the link below. I will reach out to see if that statistic is available and list it as soon as I hear back.

7153 - Incandescent Lamp T 3/4 Wire Terminal Clear 40000 Hrs 5V | HMI Components | VCC

Thank you
Ryan

I could not find direct information on the cold (room temperature) resistance of the CM-7153.

However, there is some information available with which one can make a rough calculation of it’s approximate value.

First, from the datasheet that @ryan_urness provided, it can be found that at steady-state with 5V applied, it draws approximately 0.115A, so when hot, its resistance is about 43.5 Ohms (5V / 0.115A) and will draw about 0.575W (5V x 0.115A). It also states that the M.S.C.P (mean spherical candlepower) is about 0.150 MSCP

From the same company, VCC, I found this document, Incandescent Lamp Application Information, which discusses the characteristics of tungsten miniature bulbs.

On page 4 of the above mentioned document it shows the following graph which gives color temperature for a given MSCP per Watt value:

Since the lamp has an MSCP of 0.15 and the power drawn is 0.575W, the MSCP per watt is about 0.26 (0.15MSCP / 0.575W) and the color temperature will be approximately 2150 Kelvin.

Also on page 4 of the same document, it shows a graph of relative final resistance (at steady-state) vs. resistance at room temperature for various color temperatures.

From this graph, one can see that for color temperature of 2150 Kelvin, the resistance is about 11x the room temperature value. Therefore, since the hot resistance is about 43.5 Ohms, the room temperature resistance would be about 4 Ohms (43.5 Ohms / 11).