Last week I attended the 2026 SICK Robotics Exchange Summit in Minneapolis, Minnesota.
We can summarize the major themes as:
-
The promise: Orchestration of work across a factory that includes both humans and autonomous fenceless robots.
-
The challenge: Safety standards for versatile machines working in close proximity to humans.
Terminology: Orchestration is a word used to describe the coordinated movement of work and materials across the factory floor. It includes humans, robots, and production machinery. It addresses work tasks, routes, material handoff, automated queues, temporary storage, workflow merging, inspection, and packaging.
This article is part of the DigiKey Field Guide for Industrial Automation
Location: Teach It → Industry Context
Difficulty:
System Integrator — difficulty levels explained
Author: Aaron Dahlen | MSEE | Senior Applications Engineer, DigiKey
Last update: 13 Oct 2026
Image of the idealized collaborative factory of the future (GPT generated) — with a hint of resemblance to the spaceship Cygnus.
Shape of the Factory
We begin by exploring the real-world economic pressures expressed by the group.
-
Workforce: A nearly universal concern was the lack of personnel in manufacturing. The dull, dangerous, and dirty work sentiment was expressed by several presenters as well as the fact that it is difficult to get people excited about manufacturing.
-
Flexibility and Customization: There was a time when economies of scale were the driving force behind manufacturing. The limit of this thinking is captured by Henry Ford when he implied, any color you want; as long as it’s black. That type of thinking produces a factory that is highly specialized and not well suited for retooling to produce customizable products. Consumers generally want products to match their style. A simple example is red stitching vs blue.
-
Utilization and Product Mix: Machinery that is idle is a liability. So too is machinery performing the wrong task. Consequently, it is highly desirable to quickly shift production to the most profitable products. Small CNC machine shops demonstrate this principle very well as they can generally set up quickly to accommodate a wide variety of jobs. This provides flexibility in both product and end customer. Either way, the machinery continues to run with the flexibility of accepting the jobs with the most return within the limitation of the available tooling.
Enabling Technology
It should come as no surprise that the summit was focused on the promise and challenge of AI. There is an incremental change in robotics capability enabled by AI as well as smart sensors such as vision and 3D LiDAR. While true, this group was focused on safety. That’s a huge distinction as our AI usually comes with this warning:
AI can make mistakes. Check important info.
That’s not the way to run a safety system, let alone ensure the integrity of a SIL 3 rated fenceless robot system.
Safety and Employer Responsibility
In America, we can start with OSHA’s Occupational Safety and Health Standards located in 29 CFR 1910. There we will find two important considerations:
- Requirements for safety
- Who is responsible
This was a recurring theme at the summit. While AI provides previously unobtainable functionality, the employer is still responsible for their workers’ safety.
Consequently, the entire AI functionality discussion comes down to appropriate risk reduction when we consider potential human to machine interactions. In simple words, do we “trust” that the AI and fallback systems can handle all foreseeable conditions as well as the difficult to define edge cases? Or more directly, will the employer take on additional integration, compliance validation, and maintenance complexity as opposed to traditional machine guarding?
This is no simple task in a fenceless factory with changing production. Things may look the same but the flow could change from day to day. For example, that industrial truck that normally takes a right turn now takes a left. From a human perspective this is like being a pedestrian in a country with the opposite flow of traffic. We look to the left when we should look to the right, making us oblivious to the oncoming truck—something I learned in Australia!
In fairness, many facilities already have Autonomous Mobile Robots (AMRs). The distinction is one of speed and density enabled by sensor and AI fusion. And yes, many facilities already have cobots. Again, it’s a question of speed, inertial load, and now orchestration of the work.
The presenters briefly explored the limitations of today’s standards. There was high interest in the possibility of AI being used for both the orchestration of work as well as handling an increasing amount of the safety aspects.
Resist the temptation to view this as an all-AI vs all-traditional SIL safety. Instead, ask what safety functionality can be safely passed to AI in the future: all in compliance with applicable safety standards. After all, many AMRs are not hiding behind a fence.
Tech Tip: There is an increasing interest in humanoids. They add an additional safety challenge as they are heavy and may tip over when power is lost. It was very interesting to hear the safety debate, especially when it explored humanoids with and without legs.
Challenges
This was an engineer’s summit. True to form, the edge cases were explored. Here is a sample of the conversations:
-
Communications: A surprising amount of the summit was dedicated to the limitations of communications between all of the intelligent machinery on the factory floor (emphasis on mobile equipment). At one point one of the presenters implied that robots are not the problem; keeping them running is.
-
There are challenges with mobile communications (emphasis on Wi-Fi) including bad spots, interference from large electromechanical machines, and overlapping zones with rapid switching between WAPs. This led to discussions about latency and what happens when a robot is isolated.
-
IT vs OT: Those with experience in cybersecurity placed significant importance on cybersecurity as well as reinforcing the challenges of reliable wireless coverage over the entire factory floor.
-
Little things like keeping track of time across all machines can be a problem. In one case, activating NTP on all nodes was the solution. As I understood the problem, the clock divergence across the nodes shut down the system.
-
Latency was a universal consideration. This impacts both the orchestration of work and the ability to host off-machine safety. As an example, consider the behavior of a queue of AMRs and their associated safety systems. One malfunctioning machine can negatively impact the others. Also, off-machine safety sensors can help a mobile platform see around blind corners. However, it can only do so while appropriate safety-rated communications are available between the fixed and mobile assets.
-
-
Complexity: As implied in the opening, complexity generates complexity when emphasis is placed on orchestration of custom work. As an example, consider what it takes to change work in a CNC mill. An experienced operator can change the tool, add the necessary jigs, and load the program relatively quickly. This is followed by careful measurement of test pieces and alignment. It takes time and dedicated attention to detail. We must ask how challenging it will be to perform these changes across multiple automated machines on the factory floor.
-
Equipment Repair: There were technicians after my own heart present at the summit. They pointed out the challenge of traditional troubleshooting as well as the complication of AI. Perhaps the most important consideration is the cost and long-term availability associated with AI orchestration and safety systems. And let’s not forget the cost of downtime or degraded performance if AI systems require attention, especially if the work extends into the factories IT infrastructure.
Parting Thoughts
I thank SICK Sensor Intelligence for hosting the event in their beautiful Minneapolis headquarters building.
Once again, I encourage you, dear reader, to think of AI as an incremental technology that expands a long-term trend for both orchestration of work as well as safety.
I look forward to reading the sensor fusion datasheets.
About this Author
Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.
Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.
Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.