# Configuring the MAX17205 Fuel Gauge Without Writing to Nonvolatile Memory

**URL:** <https://forum.digikey.com/t/configuring-the-max17205-fuel-gauge-without-writing-to-nonvolatile-memory/13122>\
**Category:** Integrated Circuits (ICs)\
**Tags:** analog-devices-maxim-integrated, tech-tips, power-management-pmic\
**Created:** [March 29, 2021, 3:31pm UTC](https://forum.digikey.com/t/configuring-the-max17205-fuel-gauge-without-writing-to-nonvolatile-memory/13122 "2021-03-29T15:31:37Z")\
**Posts on this page:** 1\
**Showing post:** 5

<div class="post-metadata">

**Author:** ![Matt\_Mielke](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/matt_mielke/32/71373_2.png) [@Matt\_Mielke](https://forum.digikey.com/u/Matt_Mielke)\
**Post date:** [June 8, 2021, 6:56pm UTC](https://forum.digikey.com/t/configuring-the-max17205-fuel-gauge-without-writing-to-nonvolatile-memory/13122/5 "2021-06-08T18:56:56Z")

</div>

In that case, I would start with the example I provided. In my application, I was reading voltage, current, and capacity. You’ll have to make some changes though as my application utilized two cells and their nominal capacity is likely not the same as your cell. Compare my register settings with the descriptions in the [datasheet](https://datasheets.maximintegrated.com/en/ds/MAX17201-MAX17215.pdf) to see the changes I made from the default configuration.

As for basic registers, I would start with nConfig, nNVCfgx, and nPackCfg.

Here’s the complete code from my application if that helps. Sorry about the lacking comments.

```cpp
/ ****************************************************************************** /
/* Includes */
/ ****************************************************************************** /
#include "mbed.h"

/ ****************************************************************************** /
/* Globals */
/ ****************************************************************************** /
I2C max17205( D7, D10 ); // PF_0 and PA11
Serial data_out( PB_6, PB_7, 9600 );
Ticker tick;
DigitalOut led( LED1 );

const int slave_addr = 0x6C;
const int nslave_addr = 0x16;

/ ****************************************************************************** /
/* Function Prototypes */
/ ****************************************************************************** /
int read_reg( int addr );
void write_reg( int addr, int value );

/ ****************************************************************************** /
/* Interrupt Service Routines */
/ ****************************************************************************** /
void wake( void )
{
    SCB->SCR &= ~( SCB_SCR_SLEEPONEXIT_Msk );
}

/ ****************************************************************************** /
/* Function Definitions */
/ ****************************************************************************** /
/ *******************************************************************************
* Function: main 
* Author: Matt Mielke
* Description:      
* Date: 04/03/17
******************************************************************************* /
int main( void )
{
    float RepSOC; //, VCell;
    //int Current;
    char data_str[100];

    wait( 0.5 );
    write_reg( 0x18E, 0x0A05 ); // nODSCTh
    write_reg( 0x18F, 0x4040 ); // nODSCCfg
    write_reg( 0x19E, 0x9658 ); // nVEmpty
    write_reg( 0x1B0, 0x0215 ); // nConfig
    write_reg( 0x1B3, 0x3454 ); // nDesignCap
    write_reg( 0x1A5, 0x3454 ); // nFullCapNom
    write_reg( 0x1B5, 0x0C02 ); // nPackCfg
    write_reg( 0x1B8, 0x0930 ); // nNVCfg0
    write_reg( 0x1B9, 0x080E ); // nNVCfg1
    write_reg( 0x1C0, 0xD996 ); // nVAltTh
    write_reg( 0x1C1, 0x2305 ); // nTAlrtTh
    write_reg( 0x1C2, 0x6401 ); // nSAlrtTh
    write_reg( 0x1C3, 0x00BC ); // nIAlrtTh
    write_reg( 0x0BB, 0x0001 ); // fuel gauge reset
                
    wait( 0.5 );
    tick.attach( &wake, 5.0 );
    
    while ( 1 )
    {
        led = 1;
    
        RepSOC = read_reg( 0x006 ) / 256.0;
        //VCell = read_reg( 0x009 ) * 0.078125e-3;  
    
        //Current = read_reg( 0x00A );
        //if ( Current & 0x00008000 ) Current |= 0xFFFF0000;
        
        //sprintf( data_str, "%f, %f, %f\n\r", RepSOC, VCell, Current * 1.5625e-6 / 0.0197 );

        data_out.printf( "%03.1f\0", RepSOC );
        
        led = 0;
    
        SCB->SCR &= ~( SCB_SCR_SLEEPDEEP_Msk );
        SCB->SCR |= SCB_SCR_SLEEPONEXIT_Msk;
        __WFI();        
    }
}

/ *******************************************************************************
* Function: read_reg 
* Author: Matt Mielke
* Description: This function utilizes the mbed I2C library to read the value
* contained in a register on the MAX17205. It distinguishes 
* between the volitile and non volitile address spaces. If an 
* error occurs when writing the desired address to the device, the
* write function will be repeaded until it succeeds. If the 
* subsequent read operation fails, a value of -1 is returned.  
* Date: 04/03/17
******************************************************************************* /
int read_reg( int addr )
{
    char buffer[2] = {0};
    
    if ( addr & 0x100 )
    {
        addr &= 0xFF;
        while ( max17205.write( nslave_addr, (char*)&addr, 1 ) );
        if ( max17205.read( nslave_addr, buffer, 2 ) )
        {
            return -1;
        }
    }
    else
    {
        addr &= 0xFF;
        while ( max17205.write( slave_addr, (char*)&addr, 1 ) );
        if ( max17205.read( slave_addr, buffer, 2 ) )
        {
            return -1;
        }
    }
    
    return ( buffer[1] << 8 ) | buffer[0];
}

/ *******************************************************************************
* Function: write_reg 
* Author: Matt Mielke
* Description: This function utilizes the mbed I2C library to write to a 
* register on the MAX17205. If the register address is in the non
* volitile space, the non volitile address is used. The write 
* function will repeat in a loop if it fails. 
* Date: 04/03/17
******************************************************************************* /
void write_reg( int addr, int value )
{
    char buffer[3] = {0};
    
    buffer[0] = addr & 0xFF;
    buffer[1] = value & 0xFF;
    buffer[2] = ( value >> 8 ) & 0xFF;
    
    if ( addr & 0x100 )
    {
        while ( max17205.write( nslave_addr, buffer, 3 ) );
    }
    else
    {
        while ( max17205.write( slave_addr, buffer, 3 ) );
    }
}

```

---

_[View the full topic](https://forum.digikey.com/t/configuring-the-max17205-fuel-gauge-without-writing-to-nonvolatile-memory/13122)._