Confirmation on the GENERAL CABLE#C2462A.*.10 Cable Jacket OOS

Hi Digi-Key Team,

Our production have found an issue regarding GENERAL CABLE#C2462A.*.10,the nominal OD being out of specification (OOS). Should be the dimension is 4.14mm but the actual measurement of some segment of the cable is 3.72mm and some of them is correct which is 4.14mm. Please refer to the photos below.
Is there any tolerance for the cable dimension?
Please help to review and advise on this matter.

Greetings,

“Nominal” values are approximate, and do not constitute a product specification.

Also, it may be seen in the image above that the cross-section of the cable material is not perfectly round. Some variation in measurements may be expected for this reason alone.

Hi Rick,

Then is it considered a valid reject or we have to proceed to Use As Is (UAI)

Use it as is.

Hi Rick,

For clarification, does this means that the cable did not have any allowable min/max tolerance range?

The word “nominal” refers to a thing in name, thought, generality, or custom, and is used particularly to disclaim any representation of an applicable measurement tolerance.

No min/max tolerances apply.