Cross-reference components TO 247

Hello

I have a few components to replace because I don’t know which ones are bad.

Original

KSF60F60B diode TO247

2SK1573 N-ch Mosfet TO247

FGW60N65WD IGBT TO247
2SJ352 P-ch Mosfet TO247

The ones I found

VS-60APU06-N3 Diode

TK20N60W,S1VF N-ch
AFGY100T65SPD IGBT
IRFP9240PBF P-ch

I found the P-ch Fet pins are not a match

but I dont know if I can locate better parts

Hello Power1,
Welcome to the DigiKey TechForum.
I’m glad you were able to find some alternates.
I checked for a cross for the 2SJ352 P-CH Mosfet, but I was unable to find any possible match with the same pinout, in the order of #1=Gate, #2=Source, #3=Drain.
If you can insulate and bend the wires in the correct location for the IRFP9240PBF, you have to be careful, because the mounting hole is isolated, but the metal pad on the back will still be connected to the Drain, instead of the Source, so it can not be attached to the same spot, which will probably short out the mosfet or the system.