Created by Robert Nelson, last modified on Apr 20, 2020
Introduction
This page will show you a step-by-step procedure on how we configured our XBee3 Zigbee 3.0 network at Digi-Key: LIVE DATA
Hardware Requirements
XBee End Device:
- XBee SMT Grove Development Board at Digi-Key
- XBee 3, 2.4Ghz Zigbee 3.0, U.FL Ant, SMT at Digi-Key
- Digi 2.4Ghz Whip, U.FL Ant at Digi-Key
- DFRobot SEN0291 INA219 Current Voltage Sensor at Digi-Key
XBee Gateway:
- XBee SMT Grove Development Board at Digi-Key
- XBee 3, 2.4Ghz Zigbee 3.0, U.FL Ant, SMT at Digi-Key
- Digi 2.4Ghz Whip, U.FL Ant at Digi-Key
Gateway Server:
- BeagleBone Green at Digi-Key
Software:
XBee Network Design
Product Family | XB3-24 |
---|---|
Function Set | Digi XBee3 Zigbee 3.0 |
Firmware version | 1009 |
Network PAIN ID | 5432 |
End Device XBee:
XBee End Device:
- XBee SMT Grove Development Board at Digi-Key
- XBee 3, 2.4Ghz Zigbee 3.0, U.FL Ant, SMT at Digi-Key
- Digi 2.4Ghz Whip, U.FL Ant at Digi-Key
- DFRobot SEN0291 INA219 Current Voltage Sensor at Digi-Key
Software:
XCTU Configuration
AT Commands | Parameter | Description | |
---|---|---|---|
ID | Extended PAN ID | 5432 | The preconfigured Extended PAN ID used when forming or joining a network. |
JN | Join Notification | 1 | Broadcast Join Notification upon successful join attempt. |
KY | Link Key | 00 | |
NK | Trust Center Network Key | 00 | |
NI | Node Identifier | Power_Controller | The node identifier is a user-defined name or description of the device. |
BD | UART Baud Rate | 57600 [6] | This command configures the serial interface baud rate for communication between the UART port of the device and the host. |
AP | API Enable | MicroPython REPL [4] | API enabled (operate in Micropython mode) |
PS | MicroPython Auto Start | Enable [1] | Run stored Python code at startup. |
FK | File System Public Key | Solar_Project_public_key.pem | |
D1 | DIO1/AD1 Configuration | I2C SCL [6] | Application uses I2C to talk to sensors |
P1 | DIO11 Configuration | I2C SDA [6] | Application uses I2C to talk to sensors |
Application
This devices reads a 4 INA219 Current sensors, a quick example application is show in this code block, but the full application can be found here:
from ina219 import INA219
from machine import I2C
import sys
import xbee
import time
print("#Booting Up...")
# Instantiate an I2C peripheral.
i2c = I2C(1)
for address in i2c.scan():
print("- I2C device found at address: %s" % hex(address))
while xbee.atcmd("AI") != 0:
print("#Trying to Connect...")
time.sleep(0.5)
print("#Online...")
TARGET_64BIT_ADDR = b'\x00\x13\xA2\x00\x41\xA7\xAD\xBC'
def read_battery():
try:
battery_voltage = str(battery_ina.voltage())
battery_current = str(battery_ina.current())
print_battery = "Battery:" + time_snapshot + ":BusVolt:" + battery_voltage + "V:Current:" + battery_current + "mA:#"
except:
print_battery = "Battery:" + time_snapshot + ":BusVolt:INVALID:Current:INVALID:#"
print("INA219:0x44: Battery read failed...")
try:
xbee.transmit(TARGET_64BIT_ADDR, print_battery)
except:
print("XBee: Battery TX Failed...")
battery_ina = INA219(0.1, I2C(1), 0x44)
try:
print("INA219:0x44: Configuring Battery...")
battery_ina.configure_32v_2a()
except:
print("INA219:0x44: Battery Missing...")
while True:
time_snapshot = str(time.ticks_cpu())
read_battery()
time.sleep(6)
Data Packet:
Battery:806294605:BusVolt:13.188V:Current:25.0mA:#
Coordinator XBee:
XBee Gateway:
- XBee SMT Grove Development Board at Digi-Key
- XBee 3, 2.4Ghz Zigbee 3.0, U.FL Ant, SMT at Digi-Key
- Digi 2.4Ghz Whip, U.FL Ant at Digi-Key
Software:
XCTU Configuration
AT Commands | Parameter | Description | |
---|---|---|---|
CE | Device Role | Form Network [1] | Form Network (SM must be 0 to set CE to 1) |
ID | Extended PAN ID | 5432 | The preconfigured Extended PAN ID used when forming or joining a network. |
KY | Link Key | 00 | |
NK | Trust Center Network Key | 00 | |
NI | Node Identifier | Network_Gateway | The node identifier is a user-defined name or description of the device. |
BD | UART Baud Rate | 57600 [6] | This command configures the serial interface baud rate for communication between the UART port of the device and the host. |
AP | API Enable | MicroPython REPL [4] | API enabled (operate in Micropython mode) |
PS | MicroPython Auto Start | Enable [1] | Run stored Python code at startup. |
FK | File System Public Key | Solar_Project_public_key.pem |
Application
This device just runs as an echo server, all data it receives over the ZigBee network is echoed back over the serial port to the end server (BeagleBone Green in this example), with the FROM address pre-pended to the line,
import xbee
import time
print("#Booting Up...")
while xbee.atcmd("AI") != 0:
print("#Trying to Connect...")
time.sleep(0.5)
print("#Online: Waiting for XBee messages...")
while True:
received_msg = xbee.receive()
if received_msg:
# Get the sender's 64-bit address and payload from the received message.
sender = received_msg['sender_eui64']
payload = received_msg['payload']
print("MsgFrom:%s:%s" % (''.join('{:02x}'.format(x).upper() for x in sender), payload.decode()))
Data Packet:
MsgFrom:0013A20041A7AE31:Battery:806294605:BusVolt:13.188V:Current:25.0mA:#
Gateway Server:
Gateway Server:
- BeagleBone Green at Digi-Key
Application
The Gateway Server is connected to XBee over USB, we need to configure the Serial port with stty. To parse the raw serial data, we use a python application called Grabserial, from which we grab the start of frame: “MsgFrom:” and end of frame “:#”. Attached is a quick echo example to accomplish this, the full version is available here.
#!/bin/bash
stty -F /dev/ttyUSB0 raw speed 57600 &> /dev/null
# Loop
while [ 1 ];
do
READ=`grabserial -d /dev/ttyUSB0 -b 57600 -m "MsgFrom:" -q ":#"`
echo "[$READ]:[`date`]"
done
}
Data Packet:
[MsgFrom:0013A20041A7AE31:Battery:806294605:BusVolt:13.188V:Current:25.0mA:#]:[Mon Apr 20 02:05:43 UTC 2020]