# Does Omron have a waterproof model (IP67) with a small operating force (OF)?

**URL:** <https://forum.digikey.com/t/does-omron-have-a-waterproof-model-ip67-with-a-small-operating-force-of/35410>\
**Category:** Switches\
**Tags:** switches, electromechanical, omron, faqs\
**Created:** [October 4, 2023, 8:43pm UTC](https://forum.digikey.com/t/does-omron-have-a-waterproof-model-ip67-with-a-small-operating-force-of/35410 "2023-10-04T20:43:01Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![AaronRollens](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/aaronrollens/32/8752_2.png) [@AaronRollens](https://forum.digikey.com/u/AaronRollens)\
**Post date:** [October 4, 2023, 8:43pm UTC](https://forum.digikey.com/t/does-omron-have-a-waterproof-model-ip67-with-a-small-operating-force-of/35410/1 "2023-10-04T20:43:01Z")

</div>

### Question:

Does Omron have a waterproof model (IP67) with a small operating force (OF)?

![Block](https://global.discourse-cdn.com/digikey/original/3X/5/5/55dcf4301ea7c5ffe6276999c26abe879bc7edff.png)

### Answer:

We have the following sealed basic switches with minimum OF, as shown in the catalog:  
・[D2VW](https://www.digikey.com/short/fdbbb0pr): OF 1.96 N / 200 gf (pushbutton), 0.59 N / 60 gf (long hinge lever)  
・[D2SW](https://www.digikey.com/short/2qv4vp7n): OF 1.77 N / 181 gf (pushbutton), 0.59 N / 60 gf (hinge lever)  
・[D2HW](https://www.digikey.com/short/q407r81f): OF 0.75 N / 77 gf (pushbutton), 0.50 N / 51 gf (long hinge lever)

![Block](https://global.discourse-cdn.com/digikey/original/3X/5/5/55dcf4301ea7c5ffe6276999c26abe879bc7edff.png)

### Explanation:

Due to the high airtightness of the sealed basic switch (IP67 specification), it is necessary to increase the release force (RF) compared to the open type because contraction of the internal air may delay the release when the temperature becomes low while it is being pushed in. As a result, sealed models generally require higher operating force than that of open types.

![Block](https://global.discourse-cdn.com/digikey/original/3X/5/5/55dcf4301ea7c5ffe6276999c26abe879bc7edff.png)

#### Product category

Switches Basic Switches

* * *

#### Classification

Usage, Applications

* * *

#### Related keywords

Basic Switch  
Sealed Basic Switch  
IP67  
Operating Force (OF)  
Release Force (RF)

![Block](https://global.discourse-cdn.com/digikey/original/3X/5/5/55dcf4301ea7c5ffe6276999c26abe879bc7edff.png)

Please visit the link below to see this product category on the Digi-Key website  
[Switches | DigiKey Electronics](https://www.digikey.com/en/products/category/switches/15)

  

This FAQ has been brought to you courtesy of

 ![image](https://global.discourse-cdn.com/digikey/original/3X/f/4/f485a70029a79ec3da7b845324595e6830f6a28e.png)  
  
  
Please click the link below to view the original FAQ