Does the motor model AK45-36 KV80 have its driver board with it or not

------Question for AK45-36 KV80 Please Put your question below------

Hi, does this specific listing (4505-AK45-36KV80-ND) include the built-in CubeMars driver board/controller and encoder (complete integrated actuator unit), or is it the bare brushless motor/gearbox without the internal drive electronics? Also, does the standard packaging come with the power and CAN communication cables? Thank you!

Hi @ahmed3zima4433, according to CubeMars’ product page for this part (4505-AK45-36KV80-ND), the packing list states the following is included:

  • AK45-36 KV80 Actuator (comes standard with a driver board) x1
  • Power Cable x1
  • Serial CAN Cable x1
  • Certificate of Conformance x1

Best regards!