EM9305BS211CS23B

------Question for EM9305BS211CS23B Please Put your question below------

Hello, which software should I use to write and program this chip?

Hello 2515074, thank you for the question! I reviewed the datasheet. It does mention some kind of SDK on page 33:

“The ARC processor is supported with a commercially available MetaWare toolkit (compiler, linker, debugger, etc). An integrated
development environment (IDE) and software development kit (SDK) customized for the EM9305 implementation, can easily be
used to link to functions embedded in ROM, implement patches, implement code in flash, and execute code from flash. A JTAG
and cJTAG debugging interface are provided in the QFN package format. The WLCSP package supports only cJTAG. The mode
is detected automatically.”

Page 37 indicates this:

“When configured for software development, software can be developed with the ARC EM7D Metaware IDE and downloaded into
flash. A software development kit (SDK) can be obtained from EM Microelectronic with supporting functions, API, and examples.
A hardware development kit (DVK) can be obtained from EM Microelectronic with the proper package version and a configurable
PCB.”

It seems that you have to get in touch with EM Microelectronic to get access to this. The contact page can be found here.

I believe that we also sell this development kit - EMDVK9305SOC for the EM9305.