Eval Board Dongle Source

I wanted to try using the Micro Crystal RV-3028-C7 demo board shown here. I bought it then realized it doesn’t come with a USB to I2C bridge (a way to drive it from a PC).

I searched the Micro Crystal website and found this demo kit which includes a PC GUI app for controlling it, a USB to I2C adapter dongle, and the demo board. The problem is, it doesn’t seem to have an orderable part number, and at this point, I only need the ELV USB-I2C dongle, since I managed to download the app and bought the demo board already.

ELV sells this dongle on their website, but it seems like they don’t won’t ship to the US.

I wonder if I could get some help from Digi-Key with putting in a request to Micro Crystal for this dongle so I can user their app and dongle board?

Greetings,

International trade is a headache…

Seems likely that the GUI could work with any similar sort of appliance that can talk I2C out the end and show up as a virtual COM port on the host though, and there’s a fair amount of such things out there, often based on something FTDI made. UMFT201XB-01 looks like one option that may be relatively cheap/simple.

Thanks! I considered whether I could make any similar dongle work. It seems like no.

The documentation from the full kit on the Micro Crystal website mentions the drivers needed for the ELV USB-I2C. Those drivers are for a particular USB to UART part. This means that the original dongle relies on a dongle construction scheme of “USB-UART-<some kind of MCU?>-I2C” scheme. And, the block diagram of the documentation also indicates this. This would tend to make the commands for outputting I2C signals unique to the ELV USB-I2C. All depending on the command structure decided by the firmware developers who were involved with producing the ELV USB-I2C. It’s not entirely impossible that another USB-I2C dongle follows exactly the same command structure, but I would have to “Easter egg” for it, sequentially attempting every one I can find in hopes that someone duplicated the command structure of the ELV USB-I2C.

It seems like things would go a lot easier if I could get DigiKey to help me out by putting in a request to Micro Crystal. Or, perhaps I could find a friend in Germany who will buy this ELV USB-I2C and ship it to me.

A virtual COM port is a software abstraction allowing programs such as an evaluation GUI to concern itself only with the content of messaging, rather than specifics of the hardware by which it occurs.

A similar hardware appliance with a corresponding driver that presents it to the host as virtual COM port should yield similar results.

Alternatively, one might employ a general-purpose logic probe type of device such as those offered by Digilent, Saleae, or others and their corresponding software tools to make the bits wiggle and interpret what comes back.

At day’s end it’s just I2C, not rocket surgery. Use whichever tool(s) you’re comfortable with.

Thanks again.

These things are true, just not particularly helpful in getting to evaluate the part without investing some development work, which defeats the purpose of a manufacturer providing evaluation materials.

If I could get my hands on the dongle mentioned, I could immediately evaluate the product.