Excited to start building CardioShield AI with the MAX32672FTHR from the Learn, Build & Win Program!

I’m excited to share that I received the MAX32672FTHR Development Board from Analog Devices through the Learn, Build & Win program powered by DigiKey in collaboration with Circuit Digest.

With this board, I’ll be building CardioShield AI—a portable, edge AI-based smart health monitoring system capable of real-time ECG analysis, heart rate and SpO₂ monitoring, fall detection, and early arrhythmia detection. The goal is to leverage the MAX32672’s low-power ARM Cortex-M4 processor and onboard peripherals to perform intelligent health analytics directly on the device without relying on continuous cloud connectivity.

Looking forward to exploring the board’s capabilities and sharing my progress, development updates, and final project with the community. Thanks to DigiKey, Circuit Digest, and Analog Devices for this opportunity!

:camera_with_flash: Attached: Photo of the DigiKey package along with the MAX32672FTHR development board.

Hello nabhonilbhattacharje,
Welcome to the DigiKey TechForum.
Glad to hear the good news.
Good luck with the projects.

Congratulations on receiving the MAX32672FTHR Development Board! :tada:

CardioShield AI sounds like a very impactful and technically challenging project. Combining ECG analysis, SpO₂ monitoring, fall detection, and edge AI on the MAX32672 is an exciting application of embedded intelligence.

I’m looking forward to following your development journey and seeing your progress. Wishing you all the best with the project—I hope everything goes smoothly!

Best wishes! :rocket:

:rocket: Project Progress Update – MAX32672FTHR Embedded Health Monitoring System

Over the past few days, I’ve been working on building an embedded health monitoring application using the Analog Devices MAX32672FTHR development board. The project has now progressed from an initial concept to a functional prototype running on the hardware.

The development environment has been configured successfully using the Analog Devices MSDK, and the firmware now builds and flashes reliably onto the board. The onboard 128×32 OLED display has been brought up using LVGL, while retaining the official SSD1306 driver from the SDK examples. A custom startup sequence has also been implemented, displaying the Analog Devices splash screen, followed by Circuit Digest, and finally my name before entering the main monitoring interface.

The project now interfaces with a DHT22 temperature and humidity sensor, displaying live temperature readings in both Celsius and Fahrenheit, along with relative humidity on the OLED. The firmware also includes automatic sensor updates and basic error handling for sensor communication failures.

Motion sensing capabilities have been added through the MPU6050 inertial measurement unit. The system continuously acquires 3-axis accelerometer and 3-axis gyroscope data, which are presented on the OLED through a rotating information dashboard. A software-based fall detection mechanism has also been incorporated that monitors sudden changes in motion. When a potential fall is detected, the onboard red LED blinks as a visual alert, and the OLED immediately switches to a dedicated “Fall Detected” warning screen until motion stabilizes.

To make the limited OLED display more informative, the interface has been designed as a lightweight slideshow that cycles through different pages, including environmental readings, motion data, and system status. This approach allows multiple sensor values to be viewed without overwhelming the small display.

The firmware has been organized into modular components to simplify maintenance and future development. Separate modules manage the display, sensor interfaces, motion detection, and overall application control, making it easier to extend the project with additional peripherals while keeping the codebase clean and maintainable.

The next stage of development will focus on integrating a MAX30100 pulse oximeter and heart rate sensor, improving the motion detection algorithm through sensor fusion, optimizing power consumption, and expanding the OLED dashboard with additional physiological and system information. The objective is to evolve this prototype into a compact, real-time embedded health monitoring platform built entirely on the MAX32672FTHR ecosystem.

Hello,
Thanks and keep the updates coming!