Extended board

Hello, for repair an old equipment automotive Bosch, i need an extended board for général purpose, with 40 pins each side, where i can see it on the DigiKey site ? Because i saw for larger and small one but not for 2 x 40 pins.

Thank’s

Hi mc237875,

Welcome to the TechForum.

  • Can you elaborate a bit more on what it is you’re looking for?
  • Is it a board with pads onto which parts are soldered?
  • Does it have holes in it?
  • What sort of dimensions would you expect it to be?
  • Can you give some example part numbers or images of the general type of thing you seek, so we can try to find something for you?

sorry for my later anwser.

So i put a picture comme from Vector Electronic Technilogy, which DigiKey is a local distributor.

I try to found the same board with 40 pins each side.

Also i dont know if it is 1 inch or more, for the pins, i think on my board it is more wide.

@mc237875

The below link shows the items I had found that look to match the same type of item.
Card Extenders | Prototyping, Fabrication Products | DigiKey

So far I am not seeing that we currently carry a 40position item from Vector(or any supplier I see that we list.).

Hello,

yes i saw all the products

I think it will be easier to suggest an alternative if you mention the exact configuration. Is it 40 pins per side (80 total contacts), or 2 × 40 pin headers (2.54 mm pitch)?

it is 40 pins per side (80 total contacts) and i think it is 2.54 mm pitch

We don’t look to have that at 40 contacts per side. Closest are 36 3690-2 and 50 3690-12 which you probably saw already.

yes i saw it, so it is better to take the 50 contacts and cut for put in the 40 contacts.
Thank’s

About the 3690-12 0.125" (3.18mm), 3,18mm it is between center of two contacts ?

That is correct. The contact spacing (pitch) is 0.125" (3.18mm)