Need help finding female connector, rectangular, 9 pin.
Hello,
Welcome to the TechForum.
I believe this is part WM24384-ND and I will have the link below. Please double check the lead spacing to confirm fit.
WM24384-ND
0009508090 Molex | Connectors, Interconnects | DigiKey
Thank you
Ryan
Hi,
That looks easy to measure, you just need to measure the pin to pin spacing of the mate to confirm. The WM24384-ND is 3.96mm spacing from center of the pin to the next center.
Thank you
Ryan
I notice that the female connector has 9 contacts whereas the male headers shown in the images above have 10 pins. Is that as it should be?
I believe so I also acknowledge that but the female connector only use 9 wires so I’m assuming it prob factory. Do you know the terminals that go into the female connector?
Before we give you that, please measure the pitch (spacing from center of one contact to the center of the next contact) of the connector so we know we are looking at the right connector.
The most accurate way to do this is to measure the distance from the first to the last contact and then divide that by one less than the number of contacts. So, in the case of your female connector, measure that length and divide by 8.
Pitch = L / (9contacts - 1) = ?
Any of these contacts will work with the WM24384-ND.
Again, I would recommend that you measure the pitch and verify that your pitch is 0.156" (3.96mm).
Yes, I checked and the pitch was 3.96mm
Recommended crimple tool for terminals ?
There are 3 compatible tools recommended for the series: WM25386-ND, WM9999-ND, and WM17554-ND. Generally speaking, the least expensive tools are a little harder to work with, but are compatible. There are usually more features that help guide pins when crimping for more expensive tools.
Extractor tool for terminls? kit?
The extraction tool for these is 0011030016
@losalcanzables For future reference, many of these tools and related items can be found by scrolling down on the part page and finding associated parts/tooling. See a reference image for the information beneath the product data for WM24384-ND.
You can click the “See all” links to see different configurations of what is compatible. These often include their own associated parts. Not all parts have these features, but we do try to add associated parts when possible.