I bought a GE OUTSC3HSL25085CWTN solar-powered LED light. I need to make an extension for the cable to the solar panel so it will be located in more direct sunlight. Are these connectors available on DigiKey or elsewhere? Are the cable and connectors available as an assembly? I know I could cut the cable to make it longer, but I like the idea of making it look like the factory did it. The connector’s outside circumference is approximately 0.340" (8.63 mm) and the pins are 0.050" (1.27 mm).
Thank you for your inquiry and welcome to the community.
Those connectors/cables have custom overmolded strain reliefs, indicating those cables were specially made.
We are not going to have anything that interfaces with those connectors.