Getting Started with the Schneider Lexium Cobot: Unboxing, Hardware Setup, and Initial Commissioning
If you are looking to integrate a collaborative robot into your automation setup, Schneider Electric’s Lexium Cobot line is a highly capable platform. For my recent testing and development setup, I got my hands on the LXMRL03S0000 arm (the 3 kg payload model) and paired it with the standard LXMRL03C1000 Cabinet Controller.
Since this platform was completely new to me, with no formal training, I will be documenting everything in a multi-part series explaining what you need to know. I ran into a few undocumented networking quirks and hardware specifics right out of the gate, so to start this off, here is a practical walkthrough of the initial unboxing, physical mounting, network connection, software setup, and a critical firmware trap you need to avoid.
What’s in the Box (and What Isn’t)
Each part is sold separately, and when your shipment arrives, you will find the core components split across two boxes:
-
LXMRL03S0000: The 6-axis robotic arm, which includes a permanently attached 6-meter (19.7 ft) heavy-duty umbilical cable.
-
LXMRL03C1000: The Cabinet Controller, the wired Control Stick (teach pendant), the cabinet door key, and an EU power cable.
LXMRL03S0000 Unboxing

LXMRL03C1000 Unboxing

What is not included: The mounting hardware. You will need to source your own fasteners to secure the arm to your workstation or baseplate.
-
Mounting Pattern: The base requires four holes spaced 77.78 mm apart in a square pattern.
-
Fasteners: You need four M6 bolts. Schneider Electric recommends a property class of 12.9 or greater, tightened to exactly 15 Nm (132.8 lbf-in).
For my test setup, I bolted the arm directly to a ¾-inch sheet of plywood, sized to match the area it will be used in. I also used a 1-inch hole saw directly in the center of the bolt pattern to feed the arm’s umbilical cable down through the table, keeping the workspace completely free of cable-snag hazards.
Controller Connections and Power
Despite shipping with an EU power cable, the control cabinet uses a standard IEC 320-C13 input plug and features a wide input voltage range of 100 V AC to 240 V AC at 50/60 Hz. For North American bench testing, you can safely run the entire system off a standard wall outlet using a standard NEMA 5-15P to IEC 320-C13 cable at 120V AC 60Hz.
The main connections are located on the underside of the cabinet:
-
Plug the arm’s umbilical cable into the heavy-duty twist-lock port CN14.
-
Plug the Control Stick into port CN12.
-
Plug your AC power cable into the C14 inlet at CN11.
-
Toggle the rocker switch (S11) to turn the system on.

Tech Tip: Inside the cabinet door, there are several terminal blocks for digital and analog I/O. If you plan to wire external triggers or sensors, route your wires through the supplied rubber grommets on the bottom panel to maintain the cabinet’s IP44 environmental rating.
Network Connection
Before you can program the cobot, you need to establish a network connection between your PC and the controller. You have two options: wired Ethernet or the built-in Wi-Fi.
Option A: Wired Ethernet If you want a physical connection, do not run an Ethernet cable directly from your laptop to the controller. The network port often fails to auto-negotiate a direct PC-to-controller link. You must run the Ethernet cable from port CN13 on the bottom of the controller into an intermediary network switch, and then connect your PC to the switch. If you use this method, you can skip the Wi-Fi setup below and move straight to the software installation.
Option B: Wi-Fi Connection (Recommended for Initial Setup)
-
Boot the controller by pressing and holding the On/Off button on the Control Stick for 1 second. (Quick tip: on any of the instructed 1-second or 3-second button holds on this system, I recommend holding it for an extra second, just to ensure it fully registers).
-
Open the cabinet door with the supplied triangular key. Look for a white label on the inside of the door. This label lists the unique WiFi SSID, WiFi (WPA2) password, and default Password.
-
Connect your laptop to that specific SSID using the WPA2 password.
-
Open a web browser and navigate to
10.5.5.1. (If the page fails to load, try going to[https://www.msftconnecttest.com/index.html]to force the router login prompt). -
You are now logged directly into the Wi-Fi router inside the control box. The web server will prompt you to change both the Webserver password and the Wi-Fi password immediately.
-
Update them, and then reconnect your PC to the cobot’s network using your newly created Wi-Fi password.
Software Installation & Login
To program the cobot, you need the EcoStruxure Cobot Expert software installed on your PC.
-
Download the package from the Schneider Electric website. Note: On the download page, click on “Other versions” so you can see the previous software releases. I highly recommend downloading the older versions as well, as they may be critical for troubleshooting (explained below). Also note that these zip files contain the firmware update files for the control cabinet, but for now, we only need the software installer.
-
Extract the ZIP, navigate to the
\Software\Windowsfolder, and run the installer. (There is no macOS option, and although an Android app is included, I have not tested it yet). -
Open the EcoStruxure Cobot Expert software. It opens in a non-resizable window, which can be hard to read, so click the “…” at the top right and select Maximize to make it full screen.
-
Click the robot arm icon in the top right menu to open the connection list. Double-click your controller and hit confirm.
-
Leave the user level as Administrator.
-
The Login Password: During your first login, the password for the EcoStruxure software is simply
"Administrator". Once you log in, the software will immediately prompt you to create a new, secure password for the Administrator account. -
Once connected, close the connection window. You can now press the “Power on Robot” button, wait for the lights on the arm to flash green, and select “Enable the Robot”. A prompt will appear asking you to confirm the load settings; you can leave them blank for now and hit confirm.

“Network Error During Logging In”
Before moving forward, I need to share an undocumented software quirk that cost me an entire afternoon of troubleshooting.
I installed the latest software version (V1.7.0.61) on my laptop, but every time I tried to connect, the software immediately dropped the connection and threw a vague "network error during logging in" message. Meanwhile, a colleague had unknowingly installed an older version (V1.7.0.48) on one of our lab computers. That lab computer connected to the cobot flawlessly over the exact same network.
It turned out the cobot controller was running older 1.7.0.48 firmware out of the box. Assuming an update would fix my laptop’s issue, I used the lab computer to flash the controller up to V1.7.0.61. The update succeeded, but the moment it rebooted, the lab computer was permanently locked out with the identical network error. After hours of troubleshooting, I switched back to my laptop (running V1.7.0.61), and it connected instantly. I then updated the software on the lab computer, and immediately regained control on both computers.
Note: EcoStruxure Cobot Expert strictly enforces matching revisions between the PC software and the controller firmware. If your PC software version does not match the controller’s internal firmware version exactly, they will refuse to communicate. If you encounter persistent network login errors over an otherwise stable connection, download and install a different version of EcoStruxure Cobot Expert to find the match.
Navigating the Interface
Once you connect to your controller (logging in as Administrator), you will use two primary navigation areas:
-
The Top Menu: This is your system status hub. It contains your connection toggle, the Power and Enable buttons, the Simulation/Real Cobot toggle, and the Remote Control delegation button.
-
The Bottom Feature Bar: This houses the tabs for Programming Control (the Blockly canvas), Manual Operation (jogging), the I/O Panel, and Monitoring Information. This menu automatically hides while navigating most screens, but it can be easily accessed by clicking the small arrow icon at the very bottom center of the screen.
Setting the Home Pose (Do This First!)
Before diving too far in and jogging the robot, take note that it is currently sitting in its factory “pack pose.” I need to be able to pack the robot back up in its crate for shipping to Electronica, so we need to save this exact position right now. We will map this pose to the physical Home button on the Control Stick so anyone can pack it up later.
-
Power on and enable the robot.
-
Navigate to Settings > Safety Setting > Robot Pose.
-
In this menu, you have three options: Factory Pose, Open Pose, and Home Pose.
-
Click the pencil (Edit) icon next to Home Pose.
-
A menu will open allowing you to manually jog the robot, but since it is already exactly where we want it, simply hit Confirm.
You will now see the updated coordinates saved. To test it, press and hold Move To Target Point on the Open Pose and watch the arm extend, then press and hold it for the Home Pose to verify it folds safely back into the packing position.
This concludes with the initial unboxing and setup for the LXMRL03S0000 arm and the LXMRL03C1000 Cabinet Controller. Next we need to add a grabber, and figure out how to make our first program: Part 2: Integrating a Robotiq RS-485 Gripper with the Lexium Cobot