------Question for HAC3735UF-A Please Put your question below------
Hello,
I have a question regarding the HAC3735UF-A (DigiKey Part Number: HAC3735UF-A-ND).
According to the manufacturer’s datasheet, the HAC3735 family is available with two different capacitance code options:
- H: VSUP to GND = 100 nF, OUT to GND = 1 nF
- R: VSUP to GND = 330 nF, OUT to GND = 1 nF
Could you please confirm which capacitance code is used for the HAC3735UF-A sold by DigiKey? Is it the H version or the R version?
If possible, could you also provide the complete manufacturer part number associated with this DigiKey part?
Thank you for your support.
Greetings,
The part number in question is a non-stock item (never ordered) and on first inspection does not appear to be listed at other suppliers of better repute.
Since the part number does not appear to conform to the published ordering code, my expectation is that the DigiKey listing resulted from some sort of error in our processing of price book data received from the manufacturer at some point, and isn’t actually orderable as it appears.
@comercial11
I will submit an inquiry to verify which version this item would have been meant to reference and if they can verify the order number this was meant to be.
@comercial11
This is still being worked on with the manufacturer.
@comercial11
From the information I have been given for this it looks like the HAC3735UF-A we list would be the HAC3735CXHA-2-R-4-00-HATB-070B
And they do indicate that this would be the 100nF/1nF version.