------Question for 5931 Please Put your question below------
Does it support hailo hat on rpi 5 and it has 90ohm impedance
------Question for 5931 Please Put your question below------
Does it support hailo hat on rpi 5 and it has 90ohm impedance
Which version of the Hailo Hat are you trying to replace the PCIE ribbon cable adapter on your RPI 5?
Regards,
Hailo hat 8l 13 tops to pi 5 pcie cable
Hi @rohitmarines the problem with this specific hat, RPI used a unique pcie cable:
With the connection pins on opposite sides of the ribbon..
The Pimoroni version has connections on the same side of the ribbon cable.
I haven’t found a direct replacement to date yet..
Regards,
Thank you so much …actually I am using the gpio for imu and baro .lte , gnss , mice speaker etc …so cannot mount hailo hat …need a longer cable and pin on same side
.. please suggest one which can work
The default cable provide is less then 4 cm and it has opposite contacts and when I mount the hail front side the hailo becomes upside down ..if the same length cable is there …it can still work if pin contacts are same side …
Thanks