I am interested in identifying the following 36 V battery connector. It is 4 blades in line. The pitch (distance between each pair of blades) is 6 mm, each blade is about 6.5 mm wide, the long blades are about 10 mm long, and the short ones are about 7 mm long. Only the two external (long) ones are connected. I am attaching photos of the male and female connectors.
Hello,
Thank you for contacting us.
I did look at the pictures and they will be called a Blade type power connector.
However, I am sorry, but we do not have that exact 4 pin connector. The options that we do have for 4 pins are These blade connectors
If you are able to change anything up we do have some other options that will be similar. That could include number of pins, housing style, etc. please check out These options.
As always if you have any other questions please let us know.