I’m not sure why the text didn’t show up with my pictures, but I’ll try again. I’m looking for this connect from ALTW, so Amphenol LTW, but I can’t seem to find it. The outside ring dimension is around 19mm and the inside is 11mm. It has 12 pins arranged with 9 around the outside and 3 in the middle. I looked at the Ceres Standard size and they were close, but the pins were arranged different.
I found MSAP-12BFFA-SR7001-ND that may work. The couple nut looks to be a different style though, but it may work.
Here is the drawing of the connector.
Pro_ENGINEER - MSAP-XXBFFA-SR7001.pdf (179.7 KB)
Hi, thanks so much for the suggestion but I don’t think that one will work. The pin arrangement looks right but I failed to mention the one I’m trying to match uses a 2 point locking coupling. Any chance you know of one that has the same pin arrangement and also uses the 2 point locking method?
I do not see an option with the connection type that you are looking for in our system.
Looking at the connector again, it looks like it is molded onto the cable instead of being a field wired connector.
Yes, that’s correct. It’s a molded setup.
I also checked our cable assemblies for the style that you are looking for, but I did not see any options. The options look to be all threaded.
Thanks for looking. That is what I was finding too.