Help with Chip ID

Hello All, Looking for help with this Chip ID. It is used for a 6 Hour On / 18 Hour Off Timer for LED Lights. A Crystal is attached at Pins 1 and 2, then 5V at pin 8, Neg Output to the lights at Pin 7, Gnd at Pin 4, A switch between Pins 5 & 6. The unit uses 3 AA Battery’s for power. See Photo attached.

Thanks.

@kbbeestt

I am sorry to say that I am not seeing a match for that item either.
I also did not have luck verifying the “GUID” which maybe the manufacturer of that chip.

Thanks for checking Nathan
Appreciate your time

Keith

It should look like this one.

or

1 Like