Hi guys

#1

hey guys what’s the specification of this capacitor

#2

Hello @Nareg welcome to the TechForum.

The symbol indicates that it is a Nichicon cap.
14 is a Lot code and P is 105°C
330 is capacitance which would be 330uF
35V is the voltage rating.

The only thing I can’t tell is the diameter of the cap itself. If you had that or the pad size I could id a good replacement. Short of that here are some options that meet the electrical specifications.
https://www.digikey.com/short/ppq780

-Robert

1 Like