The Switchover Circuit are used to automatically switches from the main power supply to the backup batteries.
The switchover circuit is shown in Figure 1 and is based on two LT4423 28V, 2A ideal diodes.
The backup supply is only activated when FET M1 switches off.
This function can also be achieved with two diodes. However, with a diode configuration, the highest input voltage always provides the power to the load, and if the main input is lower than the backup input, the backup supply will provide the power, which is undesirable. The two-diode solution also incurs a voltage drop that wastes input voltage and generates heat, particularly if the load current is high. Thus, an ideal diode solution is preferable.

LT4423AV#TRPBF (27V/3A (PFET) IDEAL DIODE)
Related Topics:
What is the purpose of the backup battery system in a burglar alarm?
Applicable Part Numbers
LT4423AV#TRPBF
505-LT4423AV#TRPBFCT
505-LT4423AV#TRPBFTR-ND
505-LT4423AV#TRPBFCT-ND
505-LT4423AV#TRPBFDKR-ND
505-LT4423AV#TRPBFDKR
505-LT4423AV#TRPBFTR