Below are the steps to follow when adjusting the voltage of the output module of the VCCM600 Series and further down below a demonstration video.
When setting the voltage of the output modules, the input power connector must be attached, and the unit must be powered up.
Be careful not to make contact with the input side of the unit from now on as the unit is live. The input side of the unit should be isolated to ensure safe configuration.
LEDs will illuminate on the output modules to show that they are powered up.
Set the voltage set points using a calibrated multi meter and potentiometer adjuster.
The use of shielded test leads with clips, prevents accidental shorting of the module terminals and insures a good connection.
The adjustment potentiometer on the VCCM600 Modules are recessed into the top of the output module casing.
Turning the potentiometer clockwise increases the voltage. Turning it anticlockwise decreases the voltage. For this module in this configuration set to 6V dc.
Use the potentiometer adjuster and multi meter to adjust the other modules to the required voltage.
View the demonstration video