How to program the Adafruit MEMENTO Camera Board?

The board can be programmed using Arduino or CircuitPython.

While Arduino is supported, manufacturer recommend CircuitPython because the compilation time in Arduino is pretty intense due to the huge amount of code required to run the camera.

CircuitPython is fast to develop for, and with provided libraries and examples, you can quickly build projects.

GitHub - adafruit/Adafruit_CircuitPython_PyCamera: Library for the Adafruit PyCamera · GitHub

Related Articles:
What is Adafruit MEMENTO Camera Board?
What components are included on the Adafruit MEMENTO Camera Board?
How to program the Adafruit MEMENTO Camera Board?
What expansion and connectivity options does the Adafruit MEMENTO Camera Board offer?
Does Adafruit’s MEMENTO DIY Camera Board come with SD card or cables?

image

Applicable Part Numbers

ESP32-S3
1965-ESP32-S3-ND
1528-5420-ND
5420