Out-of-band (OOB) management gives you a path to a device’s console when the production network is down. This walkthrough connects a switch console to a Connect IT 16 and covers how to reach it remotely.
What you need
- Digi Connect IT 16 (IT16-1002): 16 RJ-45 RS-232 serial ports, dual Gigabit Ethernet
- A power supply kit: ITPS-PSIK or ITPS-PSEK (required, ordered separately)
- Optional: a Digi CORE cellular module, so the console stays reachable when the LAN uplink is down (1002-CMG4-GLB)
- A standard straight-through Ethernet cable (T568B)
Steps
- Install the power supply kit and connect power. Connect an Ethernet port to your management network. DHCP is enabled by default, so you can reach the web UI at the address it receives. You can also use the included DB9-to-RJ45 adapter on the console port for local setup if you prefer.
- Connect the target device’s console port to one of serial ports 1-16. Any common straight-through Ethernet cable you have lying around should work by default, since the port pinout matches the console ports on most network gear (Cisco routers, switches, etc.). If you need the pinout, it’s in the user guide.
- Leave the serial port in its default mode and set its serial settings (baud rate, data bits, parity, stop bits) to match the target’s console settings.
- TCP, Telnet and SSH access to serial ports is disabled by default. When configuring the serial port, you can enable and configure Telnet, SSH, and raw TCP session settings on the specific ports that need them.
- Connect through Digi Remote Manager: select the device, click Actions > Open Console, and choose the serial port you want. You can also SSH to the Connect IT from the local network and pick a port from the access menu.
- With a cellular module installed, the serial consoles stay reachable over cellular when the Ethernet uplink is down. Digi SureLink® monitors the Ethernet connection and automatically fails over to cellular in the event of a LAN outage. Read more about Digi SureLink here.
Choosing between models: the Connect IT 48 has the same features with 48 serial ports instead of 16.
Hardware:
Connect IT 16 (IT16-1002)
Connect IT 48 (IT48-1002)
Power Supply:
Cold Aisle (ITPS-PSIK)
Hot Aisle (ITPS-PSEK)