------Question for SMT45A-203 Please Put your question below------
Hello gkavipurapu, welcome to the TechForum! This item is a little difficult to find a cross due to the non-standard layout of the design. I did manage to find some potential alternates, but none with the exact landing size and specification combination. If you want something that can handle more current, I’d go with 513-1725-1-ND. This does have different inductance values, but that depends how sensitive the application is to change. The package size is 0.55 by 0.55".
If you want something with closer inductance values, the next alternate you can look at is M10159CT-ND. This does have lower current ratings in parallel and series though, so you have to take note of that. This landing size is 0.55 by 0.452". I really couldn’t find anything else with closer dimensions and values that were close enough in terms of specifications.