hello,
I was sent from this topic PocketBeagle - Linux on ARM - eewiki. Basically I followed the instructions to boot up an iMX based evaluation board. I use
https://rcn-ee.com/rootfs/eewiki/minfs/ubuntu-16.04.3-minimal-armhf-2017-12-09.tar.xz for rootfs. The board booted up fine and I logged in ok (ubuntu/tempwd, logged in from the serial port), failed to ping 8.8.8.8.
I can ping the board from other computer in the network but the board itself cannot ping because of permission issue. I know I am root, as I can do dd command, etc… I can call “ping --help” but cannot do “ping 8.8.8.8”.
I followed someone note “setcap cap_net_raw+p /bin/ping” but met with message “unable to set CAP_SETFCAP effective capability: Operation not permitted”.
I cannot find any other hints to solve this problem. Can you please help ?
By the way, when I do “sudo ping 8.8.8.8”, I was met with message “sudo /usr/bin/sudo must be owned by uid 0 and have the setuid bit set”
@eelinux
Did you connect to the network?
sudo ifconfig -a
sudo dhclient eth0
That specific ubuntu image didn’t have connman installed by default to auto connect to the network.
I’ve got a newer version ubuntu that i’m slowly rolling out, just in the process of valding/updating all pages…
You can grab it here:
https://www.digikey.com/eewiki/display/linuxonarm/A10-OLinuXino-LIME#A10-OLinuXino-LIME-Ubuntu18.04LTS
Regards,
@RobertCNelson
Yes, my board connected to the network and was assigned IP address. I can ping the board but the board cannot ping the world. There are 2 issues, first sudo command does work ( met with udo /usr/bin/sudo must be owned by uid 0 and have the setuid bit set). Second, there seems to be network permission issue, when ping 8.8.8.8 (met with icmp open socket: Operation not permitted)
Can you please share with me how you may resolve this issue by with your building rootfs ?
@eelinux
Just installed the old ubuntu 16.04.3-minimal-armhf-2017-12-09 on a DE0 Altera board.
Ubuntu 16.04.3 LTS arm ttyS0
default username:password is [ubuntu:temppwd]
arm login: ubuntu
Password:
Welcome to Ubuntu 16.04.3 LTS (GNU/Linux 4.9.78-ltsi-socfpga-r4 armv7l)
ping just works…
ubuntu@arm:~$ ifconfig -a
eth0 Link encap:Ethernet HWaddr e2:e7:c4:00:49:6b
inet addr:192.168.0.117 Bcast:192.168.0.255 Mask:255.255.255.0
inet6 addr: fe80::e0e7:c4ff:fe00:496b/64 Scope:Link
UP BROADCAST RUNNING MULTICAST DYNAMIC MTU:1500 Metric:1
RX packets:86 errors:0 dropped:0 overruns:0 frame:0
TX packets:61 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:13566 (13.5 KB) TX bytes:7953 (7.9 KB)
Interrupt:27 Base address:0x2000
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:164 errors:0 dropped:0 overruns:0 frame:0
TX packets:164 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:12200 (12.2 KB) TX bytes:12200 (12.2 KB)
ubuntu@arm:~$ ping 8.8.8.8
PING 8.8.8.8 (8.8.8.8) 56(84) bytes of data.
64 bytes from 8.8.8.8: icmp_seq=1 ttl=114 time=89.7 ms
64 bytes from 8.8.8.8: icmp_seq=2 ttl=114 time=79.0 ms
^C
--- 8.8.8.8 ping statistics ---
2 packets transmitted, 2 received, 0% packet loss, time 1001ms
rtt min/avg/max/mdev = 79.040/84.394/89.749/5.362 ms
I’d say, double check your rootfs install, the chown/chmod is critical to correct the base rootfs permissions:
sudo tar xfvp ./*-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
sudo chown root:root /media/rootfs/
sudo chmod 755 /media/rootfs/
Regards,
@RobertCNelson
Thank you for your help! I have followed your instruction again and this time the rootfs worked, both sudo and ping. It was indeed permission issue. What I did wrong was using “sudo nautilus” to open file manager and did tar extract, copy & paste rootfs to SD card everything manually by drag and drop. Apparently, this came from a windows user background