Icron compatibility of Icron 2224 (EOL) with Icron 2324

Hello,
I am evaluating the replacement of the Icron 2224 extender, which has reached end-of-life status, with the ICR2324 USB 2.0 Ranger® 2324/2344 Extenders (DigiKey Part Number 5073-ICR2324-ND)

As part of this evaluation, I would like to know if Icron 2324 is compatible with Icron 2224 without requiring a PCBA redesign. Do they share the same firmware? Could you please provide more information regarding this?

Thank you

@maria.dugartesaiz

To clarify You would be referring to the below items from L-com?
If so, It looks like the 2344 would be the direct replacement for the 2244 and also from a functionality stand point would be directly compatible. As for the PCBA / firmware question I am not sure on that as they look to nominally come in a case and be used in that manner. Would you be then taking these out of the cases and using it in a larger assembly?
If so, I would advise either contacting L-Com for the PCBA / firmware question or getting 1 of the ICR2324 for your review.

L-com contact information at the very top or bottom of either linked pages below.

Icron USB 2.0 Ranger 2244 4-Port Singlemode Duplex LC USB Extender System (10km Max) - ICR2244
Icron USB 2.0 Ranger 2344 4-Port Singlemode Duplex LC USB Extender System (10km Max) - ICR2344

Hi Maria,
Icron’s 22xx EOL notice from 27 Sep 2018 names the 2324 as the replacement for the 2224. Not a drop-in though. The 2224 has a fixed duplex LC transceiver, the 2324 takes an SFP, and REX power goes from 5V to 24V. Firmware I couldn’t establish either way, that’s one for Icron.