I hope you can determine the part number so I can order a replacement connector. The connector is a surface mount right-hand female connector with 9 through-hole pins and black insulator (color not important to me, but may inform the type of connector). It is for a ThinkPad P52 laptop motherboard, and the connector protrude flush through the computer’s case, and is an always-on connector. Etched on the cover of the connector is AllTop 1931. See photos.
Hello larryedwards,
Welcome to the DigiKey TechForum.
That looks a lot like WM10411CT-ND. There are others that have those 9 pins in link below:
USB, DVI, HDMI Connector Assemblies | Connectors, Interconnects | DigiKey
Hope that helps.